ACTION#.ACTIVE

Description

Sets whether an action is disabled or enabled. When set to 1, the action will be executed if it is valid.

Value Description
0 Action disabled
1 Action enabled

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

N/A

Range

0 to 1

Default Value

0

Data Type

Integer

Stored in Non-Volatile Memory

Yes

Variants Supported

All variants are supported.

Industrial Ethernet Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

ACTION1.ACTIVE

3900h

01h

Unsigned8

-

-

Read/Write

No

ACTION2.ACTIVE

3900h

02h

Unsigned8

-

-

Read/Write

No

ACTION3.ACTIVE

3900h

03h

Unsigned8

-

-

Read/Write

No

ACTION4.ACTIVE

3900h

04h

Unsigned8

-

-

Read/Write

No

ACTION5.ACTIVE

3900h

05h

Unsigned8

-

-

Read/Write

No

ACTION6.ACTIVE

3900h

06h

Unsigned8

-

-

Read/Write

No

ACTION7.ACTIVE

3900h

07h

Unsigned8

-

-

Read/Write

No

ACTION8.ACTIVE

3900h

08h

Unsigned8

-

-

Read/Write

No

ACTION9.ACTIVE

3900h

09h

Unsigned8

-

-

Read/Write

No

ACTION10.ACTIVE

3900h

0ah

Unsigned8

-

-

Read/Write

No

ACTION11.ACTIVE

3900h

0bh

Unsigned8

-

-

Read/Write

No

ACTION12.ACTIVE

3900h

0ch

Unsigned8

-

-

Read/Write

No

ACTION13.ACTIVE

3900h

0dh

Unsigned8

-

-

Read/Write

No

ACTION14.ACTIVE

3900h

0eh

Unsigned8

-

-

Read/Write

No

ACTION15.ACTIVE

3900h

0fh

Unsigned8

-

-

Read/Write

No

ACTION16.ACTIVE

3900h

10h

Unsigned8

-

-

Read/Write

No

ACTION17.ACTIVE

3900h

11h

Unsigned8

-

-

Read/Write

No

ACTION18.ACTIVE

3900h

12h

Unsigned8

-

-

Read/Write

No

ACTION19.ACTIVE

3900h

13h

Unsigned8

-

-

Read/Write

No

ACTION20.ACTIVE

3900h

14h

Unsigned8

-

-

Read/Write

No

ACTION21.ACTIVE

3900h

15h

Unsigned8

-

-

Read/Write

No

ACTION22.ACTIVE

3900h

16h

Unsigned8

-

-

Read/Write

No

ACTION23.ACTIVE

3900h

17h

Unsigned8

-

-

Read/Write

No

ACTION24.ACTIVE

3900h

18h

Unsigned8

-

-

Read/Write

No

ACTION25.ACTIVE

3900h

19h

Unsigned8

-

-

Read/Write

No

ACTION26.ACTIVE

3900h

1ah

Unsigned8

-

-

Read/Write

No

ACTION27.ACTIVE

3900h

1bh

Unsigned8

-

-

Read/Write

No

ACTION28.ACTIVE

3900h

1ch

Unsigned8

-

-

Read/Write

No

ACTION29.ACTIVE

3900h

1dh

Unsigned8

-

-

Read/Write

No

ACTION30.ACTIVE

3900h

1eh

Unsigned8

-

-

Read/Write

No

ACTION31.ACTIVE

3900h

1fh

Unsigned8

-

-

Read/Write

No

ACTION32.ACTIVE

3900h

20h

Unsigned8

-

-

Read/Write

No

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

40100

1

40100 (0x9ca4)

ACTION1.ACTIVE

Unsigned8

Read/Write

Yes

40101

1

40101 (0x9ca5)

ACTION2.ACTIVE

Unsigned8

Read/Write

Yes

40102

1

40102 (0x9ca6)

ACTION3.ACTIVE

Unsigned8

Read/Write

Yes

40103

1

40103 (0x9ca7)

ACTION4.ACTIVE

Unsigned8

Read/Write

Yes

40104

1

40104 (0x9ca8)

ACTION5.ACTIVE

Unsigned8

Read/Write

Yes

40105

1

40105 (0x9ca9)

ACTION6.ACTIVE

Unsigned8

Read/Write

Yes

40106

1

40106 (0x9caa)

ACTION7.ACTIVE

Unsigned8

Read/Write

Yes

40107

1

40107 (0x9cab)

ACTION8.ACTIVE

Unsigned8

Read/Write

Yes

40108

1

40108 (0x9cac)

ACTION9.ACTIVE

Unsigned8

Read/Write

Yes

40109

1

40109 (0x9cad)

ACTION10.ACTIVE

Unsigned8

Read/Write

Yes

40110

1

40110 (0x9cae)

ACTION11.ACTIVE

Unsigned8

Read/Write

Yes

40111

1

40111 (0x9caf)

ACTION12.ACTIVE

Unsigned8

Read/Write

Yes

40112

1

40112 (0x9cb0)

ACTION13.ACTIVE

Unsigned8

Read/Write

Yes

40113

1

40113 (0x9cb1)

ACTION14.ACTIVE

Unsigned8

Read/Write

Yes

40114

1

40114 (0x9cb2)

ACTION15.ACTIVE

Unsigned8

Read/Write

Yes

40115

1

40115 (0x9cb3)

ACTION16.ACTIVE

Unsigned8

Read/Write

Yes

40116

1

40116 (0x9cb4)

ACTION17.ACTIVE

Unsigned8

Read/Write

Yes

40117

1

40117 (0x9cb5)

ACTION18.ACTIVE

Unsigned8

Read/Write

Yes

40118

1

40118 (0x9cb6)

ACTION19.ACTIVE

Unsigned8

Read/Write

Yes

40119

1

40119 (0x9cb7)

ACTION20.ACTIVE

Unsigned8

Read/Write

Yes

40120

1

40120 (0x9cb8)

ACTION21.ACTIVE

Unsigned8

Read/Write

Yes

40121

1

40121 (0x9cb9)

ACTION22.ACTIVE

Unsigned8

Read/Write

Yes

40122

1

40122 (0x9cba)

ACTION23.ACTIVE

Unsigned8

Read/Write

Yes

40123

1

40123 (0x9cbb)

ACTION24.ACTIVE

Unsigned8

Read/Write

Yes

40124

1

40124 (0x9cbc)

ACTION25.ACTIVE

Unsigned8

Read/Write

Yes

40125

1

40125 (0x9cbd)

ACTION26.ACTIVE

Unsigned8

Read/Write

Yes

40126

1

40126 (0x9cbe)

ACTION27.ACTIVE

Unsigned8

Read/Write

Yes

40127

1

40127 (0x9cbf)

ACTION28.ACTIVE

Unsigned8

Read/Write

Yes

40128

1

40128 (0x9cc0)

ACTION29.ACTIVE

Unsigned8

Read/Write

Yes

40129

1

40129 (0x9cc1)

ACTION30.ACTIVE

Unsigned8

Read/Write

Yes

40130

1

40130 (0x9cc2)

ACTION31.ACTIVE

Unsigned8

Read/Write

Yes

40131

1

40131 (0x9cc3)

ACTION32.ACTIVE

Unsigned8

Read/Write

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

ACTION1.ACTIVE

40100

Unsigned8

Read/Write

-

ACTION2.ACTIVE

40101

Unsigned8

Read/Write

-

ACTION3.ACTIVE

40102

Unsigned8

Read/Write

-

ACTION4.ACTIVE

40103

Unsigned8

Read/Write

-

ACTION5.ACTIVE

40104

Unsigned8

Read/Write

-

ACTION6.ACTIVE

40105

Unsigned8

Read/Write

-

ACTION7.ACTIVE

40106

Unsigned8

Read/Write

-

ACTION8.ACTIVE

40107

Unsigned8

Read/Write

-

ACTION9.ACTIVE

40108

Unsigned8

Read/Write

-

ACTION10.ACTIVE

40109

Unsigned8

Read/Write

-

ACTION11.ACTIVE

40110

Unsigned8

Read/Write

-

ACTION12.ACTIVE

40111

Unsigned8

Read/Write

-

ACTION13.ACTIVE

40112

Unsigned8

Read/Write

-

ACTION14.ACTIVE

40113

Unsigned8

Read/Write

-

ACTION15.ACTIVE

40114

Unsigned8

Read/Write

-

ACTION16.ACTIVE

40115

Unsigned8

Read/Write

-

ACTION17.ACTIVE

40116

Unsigned8

Read/Write

-

ACTION18.ACTIVE

40117

Unsigned8

Read/Write

-

ACTION19.ACTIVE

40118

Unsigned8

Read/Write

-

ACTION20.ACTIVE

40119

Unsigned8

Read/Write

-

ACTION21.ACTIVE

40120

Unsigned8

Read/Write

-

ACTION22.ACTIVE

40121

Unsigned8

Read/Write

-

ACTION23.ACTIVE

40122

Unsigned8

Read/Write

-

ACTION24.ACTIVE

40123

Unsigned8

Read/Write

-

ACTION25.ACTIVE

40124

Unsigned8

Read/Write

-

ACTION26.ACTIVE

40125

Unsigned8

Read/Write

-

ACTION27.ACTIVE

40126

Unsigned8

Read/Write

-

ACTION28.ACTIVE

40127

Unsigned8

Read/Write

-

ACTION29.ACTIVE

40128

Unsigned8

Read/Write

-

ACTION30.ACTIVE

40129

Unsigned8

Read/Write

-

ACTION31.ACTIVE

40130

Unsigned8

Read/Write

-

ACTION32.ACTIVE

40131

Unsigned8

Read/Write

-